ScriptTaskConfigObject

class

ScriptTaskConfigObject.

ScriptTaskConfigObjectMarker

Bases: object

Every ScriptObject instance will be extended with this method.

Version added

3.5.10.0

is_task_configuration

Gets a value indicating whether this instance is a task configuration object.

Return type

bool

Returns

True if this instance is task config object; otherwise, False.

class

ScriptTaskConfigObject.

ScriptTaskObjectMarker

Bases: object

Every ScriptObject instance will be extended with this method.

Version added

3.5.10.0

is_task

Gets a value indicating whether this instance is a task object.

Return type

True if this instance is task object; otherwise, False

class

ScriptTaskConfigObject.

ScriptTaskConfigObject

Bases: ScriptTaskConfigObject.ScriptTaskConfigObjectMarker

Functionality for manipulating task configuration objects.

Version added

3.5.10.0

create_task

name

Add a task object to a task configuration.

Return type

class

ScriptTaskConfigObject.

ScriptTaskObject

Bases: ScriptTaskConfigObject.ScriptTaskObjectMarker

Functionality for manipulating task objects.

Version added

3.5.10.0

name

Name of the task.

Return type

str

kind_of_task

Kind of task.

Return type

CoDeSys.TaskConfig.KindOfTask

event_pou_guid

Guid of POU for event.

Return type

Guid

priority

Priority of the task.

Return type

str

interval

Interval of the task.

Requires the property kind_of_task to be set to KindOfTask.Cyclic or KindOfTask.ExternalEvent if the device supports it.

Return type

str

interval_unit

Unit used for the interval.

Requires the property kind_of_task to be set to KindOfTask.Cyclic or KindOfTask.ExternalEvent if the device supports it.

Return type

str

watchdog

Settings for the watchdog of the task.

Return type

event

Use event to trigger the task.

Requires the property kind_of_task to be set to KindOfTask.Event or KindOfTask.Status.

Return type

str

external_event

Use external event to trigger the task.

Requires the property kind_of_task to be set to KindOfTask.ExternalEvent.

Return type

str

core_binding

Core binding. On multicore deivce each task can have an optional core binding.

Return type

int

parent_synchron_task

Task of the device application which allows synchronous calls to child application in bus cycle.

Requires the property kind_of_task to be set to KindOfTask.ParentSynchron.

Return type

str

pous

Collection of POUs which are executed by the task.

Return type

ScriptObjectCollection

class

ScriptTaskConfigObject.

ScriptWatchdog

Bases: object

A configuration for a watchdog.

Version added

3.5.10.0

enabled

Enable the watchdog for a task.

Return type

bool

time

Time monitoring for a task.

Return type

str

time_unit

Unit user for the time.

Return type

str

sensitivity

Sensitivity of the watchdog.

Return type

str

class

ScriptTaskConfigObject.

ScriptPouObjectCollection

Bases: list

A collection of POUs which are executed by a task.

Version added

3.5.10.0

add

pou_name

comment=None

Add a POU to the list.

Parameters
  • pou_name (str) -- Name of the POU.

  • comment (str) -- Optional comment about this entry

insert

index

pou_name

comment

Insert a POU to the list at the specified index.

Parameters
  • index (int) -- Index of a POU at which a new POU should be inserted.

  • pou_name (str) -- Name of the POU.

  • comment (str) -- Optional comment about this entry

replace

index

pou_name

comment

Replace the POU in the list at the specified index.

Parameters
  • index (int) -- Index of a POU which should be replaced.

  • pou_name (str) -- Name of the POU.

  • comment (str) -- Optional comment about this entry

remove

index_or_name

Remove a POU from the list at the specified index OR: Remove the first POU with the specified name from the list.

Parameters

index_or_name (int or str) -- Index or name of a POU which should be removed.