SysFileOpen (FUN)

FUNCTION SysFileOpen : RTS_IEC_HANDLE

Open or create file. A standard path will be added to the filename, if no path is specified in the file name.

If a file extension is specified in the settings, this path will be used (see category settings).

Note

File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)!

InOut:

Scope

Name

Type

Comment

Return

SysFileOpen

RTS_IEC_HANDLE

Handle to the file or RTS_INVALID_HANDLE if failed

Input

szFile

STRING

File name. File name can contain an absolute or relative path to the file. Path entries must be separated with a Slash (/) and not with a Backslash (\)!

am

ACCESS_MODE

Requested access mode to the file. See ACCESS_MODE for details.

Here find some examples:

AM_READ

If file does not exist, an error is returned. If the file exists, the file will be opened

AM_WRITE

If file does not exist, a new file will be created. If the file exists, it will be overwritten!

AM_APPEND

If the file does not exist, an error is returned. If the file exists, the file will be opened

pResult

POINTER TO RTS_IEC_RESULT

Pointer to runtime system error code (see CmpErrors.library)