FUNCTION_BLOCK PID_FIXCYCLE
Represents a PID controller for which the cycle time can be set manually
A PID controller continuously calculates an error value e(t) as the difference between a desired set point and a measured process variable. The PID contoller applies a correction based on proportional, integral, and derivative terms (sometimes denoted P, I, and D respectively) which give their name to the controller type.
For fast and fix tasks it is recommended to use PID_FIXCYCLE instead of PID, because the cycle time is defined accurately, whereas PID only can measure the cycle time with a maximum accuracy of milliseconds. In case of very short cycles (1ms) this might lead to a rough run (see PID).
It is not necessary to readjust the controller parameters (KP, TN, TV) if the cycle time changes.
For more information see: PID.
| InOut: |
|