WORD_AS_BIT (FB)

FUNCTION_BLOCK WORD_AS_BIT

Converts an input value of data type WORD into 16 outputs of data type BOOL

InOut:

Scope

Name

Type

Comment

Input

W

WORD

Input value

Output

B00

BOOL

Output bit 0

B01

BOOL

Output bit 1

B02

BOOL

Output bit 2

B03

BOOL

Output bit 3

B04

BOOL

Output bit 4

B05

BOOL

Output bit 5

B06

BOOL

Output bit 6

B07

BOOL

Output bit 7

B08

BOOL

Óutput bit 8

B09

BOOL

Output bit 9

B10

BOOL

Output bit 10

B11

BOOL

Output bit 11

B12

BOOL

Output bit 12

B13

BOOL

Output bit 13

B14

BOOL

Output bit 14

B15

BOOL

Output bit 15