Command 'Renumber CNC program'

Symbol:

Function: This command refreshes the numbering of program lines in the CNC program.

Call: Menu bar: CNC .

Requirement: A CNC path is open in the editor.

The numbers start at 0 and are incremented by 10. Each block without a block number receives a number. L code in G20 blocks is corrected.

See also