CODESYS provides the capability of creating CNC programs in two different editors: the editor for DIN 66025 and the tabular editor. Both editors display a graphical view of the programmed path.
Although programming can be exchanged between the editors, this can lead to information losses.
Element |
Editor for DIN 66025 |
table editor |
---|---|---|
Positioning |
X |
X |
Line |
X |
X |
Arc |
X |
X |
ellipse |
X |
X |
Spline |
X |
X |
Rapid positioning |
X |
X |
M function |
X |
X |
Parabola |
X |
|
Using Variables |
X |
|
Jump |
X |
|
Coordinate shift |
X |
|
step suppression |
X |
|
Dwell time |
X |
|
Timing synchronization with interpolator |
X |
See also