The Selective Compliance Assembly Robot Arm (SCARA) is a special type of industrial robot that is similar to a human arm. A SCARA system has two axes and two degrees of freedom. The movement is restricted to the X/Y plane.
See also
SMC_TRAFO_Scara2 (FB)
SMC_TRAFOF_Scara2 (FB)