Dialog 'New Connection'

Generic connection (freely configurable)

The dialog contains the parameters for the new connection.

Connection Path Settings

Automatically generated path

The Connection Path is generated automatically from the values for Configuration assembly, Consuming assembly, and Producing assembly.

User-defined path

The Connection Path is specified manually in the corresponding input field.

Path defined by symbolic name

The path is specified by a symbolic name.

Requirement: The device must support symbolic connection paths.

General Parameters

Connection Path

The connection path is used to address one or more objects in the adapter that provide the input data and receive the output and configuration data.

Requirement: The connection path is set to User-defined path.

Symbolic name

An ANSI string is used instead of the normal connection path. See the manual of the respective EtherNet/IP adapter for permitted ANSI strings.

Requirement: The connection path is set to Path defined by symbolic name.

Trigger type

  • Cyclic: Data exchange takes place cyclically at intervals set by the RPI.

  • Change of State: Data is exchanged automatically after a change to the scanner outputs or adapter inputs.

  • Application: Not implemented

Transport type:

Details for this can be taken from the specifications CIP Volume 1 and Volume 2.

RPI (ms)

(Requested Packet Interval) Length of the time interval (in milliseconds) in which the transmitting application requests the transmission of data to the target application. This value must be a multiple of the bus cycle task.

Timeout multiplier

In case of device failure, there is a time delay (RPI * Timeout multiplier) before the device state switches to "Error".

Predefined connection (EDS file)

Use this option to employ existing connections from an EDS file. The data that can be changed are defined in the EDS file.

Scanner to Target (Output)

O--> T size (bytes)

Amount of data from scanner to adapter

Proxy Config Size (Bytes)

Size of proxy configuration data

Target Config Size (Bytes)

Size of target configuration data

Connection type

  • Null: A network connection is not established.

  • Multicast: A network connection is established. The connection data can be received by multiple consumers.

  • Point to Point: A network connection is established. The connection data can be received by exactly one consumer.

Connection Priority

Two scanners using different priorities to one target can cause conflicts. Adapting the connection priority solves this problem.

Fixed/Variable

See the specifications CIP Volume 1 and Volume 2 for details of the parameters.

Transfer format

Inhibit time

Heartbeat multiplier

Requirement: The Transfer format is Heartbeat.

Extends the interval at which the scanner sends heartbeat messages to the adapter. This value is multiplied by the RPI value.

Example: RPI = 10ms and Heartbeat multiplier = 10 causes a message to be sent every 100ms.

Target to Scanner (Input)

T--> O size (bytes)

See description for Scanner to Target.

Connection type

Connection Priority

Fixed/Variable

Transfer format

Inhibit time

See also