Tab 'EtherNet Adapter - General'

Object: Ethernet Adapter

This tab defines the network interfaces.

Network interface

: Opens the Network Adapters. The Ethernet adapters can be selected here, which are available on the set target system.

IP address

Subnet mask

Default gateway

Settings of the selected network interface

Adjust operating system settings

You must confirm this option again.

Note: The settings on the target system will be overwritten by the values above.

The IP settings of the operating system can be changed by the CODESYS runtime system only if this is permitted in the configuration file (*.cfg) of the runtime. The following entries are required for this:

[SysSocket]

adapter.0.name="<adapter name>" (for example, "LAN Connection 4")

Adapter.0.EnableSetIpAndMask=1

See also

Dialog 'Network Adapters'

Interfaces

Shows an overview of all available network adapters.

IP address

Subnet mask

Default gateway

These parameters are taken from the operating system and cannot be modified.

MAC address

MAC address of the Ethernet adapter