IO-Link Configurator

Note

Refer to the general description for information about the following tabs of the device editor.

  • Tab '<device name> I/O Mapping'

  • Tab '<device name> IEC Objects'

  • Tab '<device name> Parameters'

  • Tab '<device name> Status'

  • Tab '<device name> Information'

Only in the case of special features is there an additional help page for the specific device editor.

If the "<device name> Parameters" tab is not shown, then select the Show generic device configuration editors option in the CODESYS options (Device Editor category).

IO-Link is a communication system for the linking of intelligent sensors and actuators to an automation system. An IO-Link system consists of an IO-Link master that provides the interface to the higher-level controller (PLC) and one or more IO-Link devices (sensors and actuators).

The associated IODD device description files must be installed in the device repository before the IO-Link modules are available in the 'Set device' dialog.

3.5.15.0

© Copyright 2021, CODESYS GmbH