Command 'Scan for Devices'

Function: This command establishes a brief connection to the hardware and determines the devices in the network. You can then adopt the devices found into the device tree of your project.

Call: Main menu Project , context menu of a device object in the device tree.

Requirement: The settings for communication with the control device are correct. The gateway and the PLC are running. The device supports the scan function.

The following devices provide the scan function: EtherCAT, EtherNet/IP (IEC), Sercos, CANopen, PROFINET, PROFIBUS DP.

Note

You can perform the scan immediately if the scan function is permanently implemented in the PLC. If scan function is located in a library, you must log in once in order to load the library to the controller.

The command refers to the master controller selected in the device tree. For example, an already inserted PROFINET IO controller can be selected and the command used to determine the I/O devices and I/O modules assigned to it.

After scanning, the dialog box Scan for Devices appears with the results.

Dialog 'Scan Devices'

Scanned Devices

Device name, Device type, Address, Station name, etc.

Data about the scanned device depending on network type.

When you change a value in the list of scanned devices, the value is shown in italics. This indicates that the new value has been changed in the editor in CODESYS, but not in the device. When you download the value to the device, it is shown normally.

Value that indicate differences between the project and the scanned device are shown in orange.

If several device descriptions are available for the scanned device, then the name is displayed in bold. The selection of the matching device description is resolved differently for different fieldbuses. Details can be found in the corresponding fieldbus sections.

If a device description cannot be found, then the following message is shown: "Attention! The device was not found in the repository." Depending on the bus system, additional information is displayed, such as manufacturer number and product number. The device cannot be inserted into the project without the installed device description.

Show differences to project

: The table in the dialog also shows additional configured devices (in the device tree of the project).

: The table shows all scanned devices. The configured devices are not shown.

Scan Devices

Starts a new search.

Copy all devices to project

The device that is selected in the table is inserted into the device tree in the project. If nothing is selected, then all scanned devices are shown.

Notice

If you insert devices, which are available in the device tree, to the device tree with Copy All Devices to Project, then the following should be noted. The data of the Process Data and <...> I/O Mapping tabs of the existing devices can be overwritten with the data of the recently inserted devices.

Configured Devices

This part of the dialog is visible only when you select the Show differences to project option.

Differences between the scanned and configured devices are color-coded. Devices in green are identical on both sides. Device in red are available only in the view of the scanned or configured devices.

If you have selected a device in both views, then the scanned devices are inserted above the selected configured device.

If you have selected a device in both views, then the scanned devices are inserted below the selected configured device.

If you have selected a device in both views, then the configured devices are replaced by the selected scanned device.

All scanned devices are copied to the project.

Deletes the selected configure device.

Special settings for PROFIBUS DP

Scan Devices

New search for devices in the PROFIBUS DP master network.

Copy all devices to project

Copies all selected slaves into the project. Existing slaves with the same address are overwritten.

State

Scanned and projected slaves are assigned by station address.

  • : The detected devices matches the configured device.

  • : No device was detected with the same station address.

  • : Assignment of the detected device to the configured device is possible, but the module configuration is different.

Unique assignment to the devices of a specific manufacturer is not possible with the available information (ID number for slaves, I/O configuration for modules). The Add Device dialog opens where you can assign the scanned devices manually to the devices available in the project.

See also