PROFIBUS DP Slave Device - 'General'

This tab is used for configuring the main settings of a DP slave for data exchange in the network.

Settings

Address:

Station address of the slave within the PROFIBUS DP network. Possible values: 1-126. Default: 126

Baud rate:

Baud rate for data exchange. Possible settings: Auto (default; baud rate as predefined from the bus master), 9,600 / 19,200 / 31,250 / 45,450 / 93,750 / 18,750 / 500 / 1500 / 300 / 600 / 12000)