Tab 'Modbus TCP Slave Device - Serial Gateway'

Object: ModbusTCP Slave Device

Note

This functionality is not included in the standard scope of the license for the Modbus TCP Slave. The Modbus Serial Master also has to be licensed.

The tab contains the settings for extending the device to a serial Modbus TCP/RTU Gateway. The Modbus TCP Slave then forwards the requests of a TCP Master to Modbus RTU Slaves which are connected to the local COM port of the PLC.

Serial Gateway Active

: The TCP/RTU gateway functionality in the device is enabled.

COM port

Number of the COM port used

Baud rate

Transmission rate (in baud)

See also