Symbol:
Function: This command opens the Visualization Styles dialog box. It makes it possible to edit visualization style repositories.
Call: Menu bar: .
See also
|
Storage location |
Name of the currently selected repository Preset: System
|
|
(...) |
Storage location of the repository
Example: |
|
Edit locations |
The Edit Repository Locations dialog box opens. |
|
Company |
When a company name is specified here, the tree view is filtered and only the styles of the selected company are listed. Preset: (All companies). It is not filtered.
|
|
Windows with styles |
Tree view of all versions of the installed visualization styles in the selected repository |
|
Display localized names |
|
|
Install |
The Select Visualization Style(s) dialog box opens. |
|
Uninstall |
The selected style version is removed from the repository. |
|
Preview |
The windows closes. A preview is displayed of the selected style in the selected version. Specific elements are displayed in the style. |
|
Location |
Storage location of the configured repository on the development system
Example: |
|
Name |
Preset: |
|
Add |
The Repository Locations dialog box opens. It makes it possible to manage other repositories. |
|
Edit |
|
|
Remove |
|
|
Move Up |
The order in the list of repositories is adapted. It defines the processing order when searching for elements. |
|
Move Down |