Setting Up User Management for Visualizations

When you set up user management for your visualization, the following variants are possible:

  • Empty user management

    An empty user management contains the None user group. You configure all users and groups yourself.

  • User management with default users and groups

    This user management contains the Admin, Service, Operator, and None groups. The first three groups each contain one user with the same name as the group.

Create new user management

Requirement: A user management does not exist yet for your visualization.

  1. Click the Visualization Manager object in the device tree.

  2. Select the User Management tab.

  3. Click Create Empty User Management or Create User Management with Default Groups and Users depending on which variant you need.

    ⇒ The Groups, Users, and Settings tabs are displayed.

    The Group tab opens.

  4. If you have created an empty user management, then you configure the new groups and users.

    If you have created a user management with default groups and users, then you can grant permissions for elements in your visualization. You can also select the user management dialogs and assign them to the buttons of the visualization.

See also