Dialog 'Create a New Visualization Style'

Symbol:

Function: The dialog prompts you to specify data for a new created style file.

Call:

  • In CODESYS:

    In the Visualization Manager object (tab Settings, group Style Settings):

    Clicking opens a drop-down list. Click Create and Edit Derived Style.

  • In the visualization style editor:

    Menu bar: File ‣ New Style

Name

Name of the new style.

Example: Style_CI

Storage location

Working directory for style editing

Base style

Style to base the new style on The drop-down list includes all styles that are installed in the repository.

<none>: The new style does not derive itself from an existing style.

Visualization profile

The profile is intended for informational purposes. For example, you find elements that are not preconfigured with special style entries, and information from the profile. In addition, CODESYS checks in the profile whether a required style is missing.

Example: CODESYS V3.5 SP9

Click OK

The new style is created and opened for editing in the visualization style editor. It already includes all required style entries and the localization in German (language column de).

See also