Dialog 'Create HMI Project - Connect to HMI Device'

Function: This dialog box is part of the wizard that opens when you create a new project with the HMI project template. This allows for optional setting of the communication parameters for the HMI device.

Call: Automatically after the Create HMI Project - Select HMI Device dialog box

See also

Gateway

List of known gateways that are active in the network.

Device

Network name of the device to establish a connection.

Select path by network scan

By clicking this button, you start the network scan and a list of all active HMI devices appears in the Select device dialog.

Active communication path

Network name and address of the selected device.

Next >

The Create HMI Project - Add Objects dialog box opens.

Abort

The configuration and settings of an HMI project are ended.

See also