The visualization editor provides the visualization elements for the design of a user interface in the view Tools.
Drag the desired element into the editor window and adapt it in the view Properties: purely visual design, labelling, display of data, reaction to user inputs, possibility to input values, etc.
Static or dynamic configuration of the properties is possible, i.e. the assignment of fixed values or application variables. A dynamic configuration allows an animation that is executed at runtime.
See also