A short description of each selected menu item is displayed in the status bar. The use of the menu items is explained in the corresponding procedures referenced in the following table.
Which items are available depends on the program part or editor you are working with.
Machine Expert – Safety can also be operated via keyboard shortcuts.
File |
Provides commands for
|
Edit |
Provides commands for
|
View |
Provides commands for
|
Project |
Provides commands for
|
Build |
Provides commands for
|
Objects |
Commands in the 'Objects' menu are only active while using the FBD/LD code editor. It provides commands to insert FBD/LD objects into the code and to modify object properties. |
Layout |
While editing code in FBD/LD code worksheets, the 'Layout' menu provides several utilities (e.g., you can display a grid). Furthermore, you can zoom into and out of the worksheet and modify the default contact/coil width. While working in a variables worksheet, the 'Layout' menu contains zoom commands and a menu item for resetting the present grid column width. |
Online |
Provides commands for
|
Window |
Provides commands for arranging windows in the workspace and closing all open windows at once. |
? |
Provides commands for calling help information. Refer to the topic "How to use the Online Help System" for detailed information. |
EIO0000002147.08