This standard bit manipulation function contained in the <BIT_UTIL> library reads the value of a particular bit in the bit string applied at input IN.
Parameter |
Data type |
Description |
---|---|---|
IN |
ANY_BIT |
Input bit string |
BIT_NO |
BYTE |
Number (position) of the bit to be read |
OUT |
BOOL |
Value of the read (tested) bit |
ANY_BIT contains the data types DWORD, WORD, BYTE and BOOL.