FUNCTION CONCAT : STRING(255)
Concatenates two strings
CONCAT(STR1,STR2) means: Connect STR1 and STR2 to a single string STR1STR2.
(* Example declaration *)
VarSTRING1 : STRING ;
(* Example in ST , result is 'SUSIWILLI' *)
VarSTRING1 := CONCAT ('SUSI','WILLI');
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Return
|
CONCAT
|
STRING(255)
|
Concatenated string, max. 255 characters. If the result doesn't fit into these 255 bytes, it will be silently truncated. No error is produced.
|
|
Input
|
STR1
|
STRING(255)
|
String 1 to be concatenated, max. 255 characters
|
|
STR2
|
STRING(255)
|
String 2 to be concatenated, max. 255 characters
|
|