CAA Segmented Buffer Manager Extern Library Documentation

Company

CAA Technical Workgroup

Title

CAA Segmented Buffer Manager Extern

Version

3.5.11.0

Categories

Intern|CAA|Runtime

Namespace

SBM

Author

3S - Smart Software Solutions GmbH

Placeholder

CAA SegBufMan

Description [1]

This library provides a set of functions for handling different segments of one huge buffer, joining segments or splitting buffers in segments. This is done without copying the content all the time. The functions try to reference the segments instead of copy them and manage the segments in double linked lists.

Indices and tables

[1]

Based on CAA_SegBufferMan_Extern.library, last modified 03.07.2017, 15:35:25. LibDoc 3.5.16.0

The content file CAA_SegBufferMan_Extern.clean.json was generated with CODESYS V3.5 SP11 on 03.07.2017, 15:35:29.