TYPE IEC_CYCLE_STRUCT : STRUCT
This struct is passed as parameter to the TaskEntryFunction, see IecTaskCreate
Name
Type
pTaskInfo
POINTER TO Task_Info2
pApplication
POINTER TO APPLICATION
hTaskHandle
RTS_IEC_HANDLE
bResult
BOOL
bDummy1