ILConTlC (ITF)

INTERFACE ILConTlC EXTENDS ILConC, ITimeLimited, ITimingControlled

In order to build a function block with a LConTlC behaviour, its action provider has to be decorated with this interface. This will determine the state machine which then forces the function block to the appropriate LConTlC behaviour.

See Decorators for more information about the concept.

A state chart for function blocks with LConTlC behaviour

Starting

StartAction is running, until xComplete is TRUE, xBusyTRUE

Executing

CyclicAction is running until xComplete is TRUE

Cleaning

CleanupAction is running. At its end the ExitAction is probably executed one time.

After a Ready Condition as input, only the output state

Error (eErrorIDERROR.NO_ERROR) is possible.

After a Error Condition as input, only the output state

Error (eErrorIDERROR.NO_ERROR) is possible.

After a Abort Condition as Input, only the output states

Resetting or Error (eErrorIDERROR.NO_ERROR) are possible.

(xBusy is still TRUE!)

Error

xErrorTRUE, eErrorIDERROR.NO_ERROR, xBusyFALSE

Resetting

ResetAction is running, until xComplete is TRUE.

After that:

- the output xError will be set to FALSE.

- The output eErrorID will be set to ERROR.NO_ERROR.