TYPE STATE :
Every state listed below is represented by an element in the state chart.
The PLCopen defines two different variables (xEnable/xExecute) for starting a function block depending on its type. For this reason a neutral name xControl has been chosen. The xControl input variable can act as a xExecute or an xEnable input variable. This depends on how the related action provider is decorated. If the action provider is decorated with IEdgeTriggered then the xControl input variable acts as an xExecute. If the action provider is decorated with ILevelControlled then the xControl input variable acts as an xEnable.
Dormant⇒ Waiting for xControl (xEnable/xExecute)
Starting⇒ StartAction is running, until xComplete is TRUE, xBusy ⇒ TRUE.
At its beginning the SampleAction is probably executed one time.
Executing⇒ CyclicAction is running until xComplete is TRUE
Cleaning⇒ CleanupAction is running.
At its end the ExitAction is probably executed one time.
After a Ready Condition as input, only the output states
Done (xComplete is TRUE) or Error (eErrorID ≠ ERROR.NO_ERROR) are possible.
After a Error Condition as input, only the output state
Error (eErrorID ≠ ERROR.NO_ERROR) is possible.
DonexDone ⇒ TRUE, xBusy ⇒ FALSE
ErrorxError ⇒ TRUE, eErrorID ≠ ERROR.NO_ERROR, xBusy ⇒ FALSE
Resetting⇒ ResetAction is running, until xComplete is TRUE.
After that:
- the outputs xDone and xError will be set to FALSE.
- The output eErrorID will be set to ERROR.NO_ERROR.
| Attributes: |
qualified_only |
||||||||||||||||||||||||||||||
| InOut: |
|