3S - Smart Software Solutions GmbH
IoDrvGPIOBBB
3.5.10.30
Intern|IoDrivers
GPIO I/O driver for BeagleBone Black
Configuration (GVL)
IoDrvGPIOBBB (FB)
IoDrvGPIOBBB.ConfigurePinAI (METH)
IoDrvGPIOBBB.ConfigurePinDI (METH)
IoDrvGPIOBBB.ConfigurePinDO (METH)
IoDrvGPIOBBB.IsChannelEnabled (METH)
IoDrvGPIOBBB.ReadPin (METH)
IoDrvGPIOBase (FB)
IBase
ICmpIoDrv
ICmpIoDrvConfig
ICmpIoDrvParameter
PinConfiguration
MemRegion (STRUCT)
PinFunction (ENUM)
[1]
Based on IoDrvGPIOBBB.library, last modified 01.01.1601, 00:53:00. LibDoc 3.5.16.0
The content file IoDrvGPIOBBB.clean.json was generated with CODESYS V3.5 SP10 Patch 4 on 12.06.2017, 10:03:58.