FUNCTION_BLOCK PUBLIC FINAL TCP_Read EXTENDS LConC
This function block serves to read data from the previously established connection given in itfConnection. As long as xEnable is TRUE and the connection is valid. The pointer pData specifies the memory area to write the read data to. udiSize defines the max number of bytes to read. When the data was read successfully, xReady is set to TRUE and udiCount indicates the actually read number of bytes.
InOut: |
|