IecLanguageObjectContainer

class

IecLanguageObjectContainer.

PouType

Bases: enum.Enum

Defines the type of the POU which is to be created.

Version added

3.5.9.0

Program

= 1

A Program.

FunctionBlock

= 2

A function block.

Function

= 3

A function.

class

IecLanguageObjectContainer.

DutType

Bases: enum.Enum

Defines the type of the DUT which is to be created.

Version added

3.5.9.0

Structure

= 1

A structure.

Enumeration

= 2

An enumeration.

Alias

= 3

An alias.

Union

= 4

An union.

EnumerationWithTextList

= 5

An enumeration with integrated text list support.

class

IecLanguageObjectContainer.

ScriptIecLanguageObjectContainer

Bases: object

This allows objects to create POU like objects, the methods will be available in the project root as well as applications, and folders below them.

The extended settings and specializations which are available in the "Add Object" dialog, but not available in this interface, can be implemented by direct access of the textual declaration part via ScriptObjectWithTextualDeclaration - for example, setting derived interfaces, or persistent or constant GVLs.

Version added

3.5.9.0

create_pou

name=None

type=<PouType.FunctionBlock: 2>

language=None

return_type=None

base_type=None

interfaces=None

Creates a POU with the specified name and type.

 WARNING

The original C# function that is called with this method contains 2 overloads. It is strongly advised to pass all arguments with their respective keywords.

create_pou(self, name, type=PouType.FunctionBlock, language=None, return_type=None, base_type=None, interfaces=None) (1/2)

Parameters
  • name (str) -- The name.

  • type (PouType) -- The type. Optional, the default is a function block.

  • language (Guid) -- The language. Optional, the default is structured text.

  • return_type (str) -- The return type. This is required for PouType.Function, and not allowed for other POU types.

  • base_type (str) -- The base type. This is optional and only allowed for PouType.FunctionBlock.

  • interfaces (str) -- The implemented interface(s). This is optional and only allowed for PouType.FunctionBlock.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created POU.

create_pou(self, type) (2/2)

Creates a POU with implicit checks according to the specified type.

Adding a check function will provoke a full recompile and prohibit an online change.

Version added

3.5.12.10

Parameters

type (SpecialPouType) -- The SpecialPouType which should be created.

Raises

Exception -- Any exception which might occur (e. G. if an object with the same name already exists within the same namespace or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created POU.

create_gvl

name

Creates a GVL with the specified name.

Parameters

name (str) -- The name.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created GVL.

create_dut

name

type=<DutType.Structure: 1>

baseType=None

Creates a DUT with the specified name and type.

As with manual object creation in the UI, enums will get the attribute 'strict' with compiler versions >= 3.5.7.0, and additionally the attribute 'qualified_only' with compiler version 3.5.8.0.

Parameters
  • name (str) -- The name.

  • type (DutType) -- The type.

  • baseType (str) -- The base type. This optional parameter is necessary for for Alias types, optional for STRUCTs and enums, and currently not allowed for unions.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created DUT.

create_interface

name

baseInterfaces='__System.IQueryInterface'

Creates an interface with the specified name.

Parameters
  • name (str) -- The name.

  • baseInterfaces (str) -- The base interfaces (comma separated).

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created interface.

class

IecLanguageObjectContainer.

ScriptIecLanguageMemberContainer

Bases: object

This allows objects to create POU like member objects, the methods will be available on POUs, Interfaces, GVLs, and folders below them.

The extended settings and specializations which are available in the "Add Object" dialog, but not available in this interface, can be implemented by direct access of the textual declaration part via ScriptObjectWithTextualDeclaration - for example, setting derived interfaces, or persistent or constant GVLs.

Version added

3.5.9.0

See also: ScriptTreeObject

create_property

name

return_type='int'

language=None

Creates a property with the specified name and type.

Parameters
  • name (str) -- The name.

  • return_type (str) -- The return type.

  • language (Guid) -- The language for the getter and setter. Optional, the default is structured text. It is illegal to specify a language for interface properties.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created property.

create_method

name

return_type=None

language=None

Creates a method with the specified name and type.

Methods cannot be added to GVLs or Functions.

Parameters
  • name (str) -- The name.

  • return_type (str) -- The return type.

  • language (Guid) -- The language for the getter and setter. Optional, the default is structured text.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created method.

create_action

name

language=None

Creates an action with the specified name and type.

Actions cannot be added to GVLs or Functions.

Parameters
  • name (str) -- The name.

  • language (Guid) -- The language for the getter and setter. Optional, the default is structured text.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created action.

create_transition

name

language=None

Creates an transition with the specified name and type.

Transitions cannot be added to GVLs or Functions.

Parameters
  • name (str) -- The name.

  • language (Guid) -- The language for the getter and setter. Optional, the default is structured text.

Raises

Exception -- Any exception which might occur (e. G. if the name is not an IEC identifier, or an object with the same name already exists within the same namespace, or the language guid is not valid, or the object cannot be created under this parent.

Return type
Returns

The ScriptObject of the newly created transition.

class

IecLanguageObjectContainer.

ScriptImplementationLanguage

Bases: object

Defines the Guids for the standard IEC 61131-3 languages and those available as CODESYS extensions.

An instance of this interface will be injected with the name "ImplementationLanguages".

Version added

3.5.9.0

st

Gets the language guid for ST / Structured Text.

Return type

Guid

cfc

Gets the language guid for CFC / Continous Flow Chart (free layout FUP).

Return type

Guid

page_oriented_cfc

Gets the language guid for Page oriented CFC / Continous Flow Chart (free layout FUP).

Return type

Guid

fbd

Gets the language guid for FBD / Function Block Diagram (FBS).

Return type

Guid

instruction_list

Gets the language guid for IL / Instruction List (AWL).

Return type

Guid

ladder

Gets the language guid for LD / Ladder Diagram (KOP).

Return type

Guid

uml_statechart

Gets the language guid for the uml statechart.

The UML AddOn needs to be installed for this language. See also: http://store.codesys.com/codesys-uml.html

Return type

Guid

class

IecLanguageObjectContainer.

SpecialPouType

Bases: enum.Enum

Defines the type of special POUs (with implicit checks) which have to be created.

Version added

3.5.12.10

none

= 1

No special POU.

check_bounds

= 2

Bound checks.

Appropriate handling of bound violations; such handling includes setting flags or changing field indices.

check_pointer

= 3

Pointer checks.

check_range_unsigned

= 4

Check range unsigned.

check_range_signed

= 5

Check range signed.

check_div_real_64

= 6

Check division real 64 bit.

check_div_real_32

= 7

Check division real 32 bit.

check_div_int_64

= 8

Check division real 64 bit.

check_div_int_32

= 9

Check division real 32 bit.

check_l_range_unsigned

= 10

L-range checks unsigned.

check_l_range_signed

= 11

L-range checks signed.