HYSTERESIS (FB)

FUNCTION_BLOCK HYSTERESIS

Realizes a hysteresis function

InOut:

Scope

Name

Type

Comment

Input

IN

INT

Input value

HIGH

INT

Upper limit

LOW

INT

Lower limit

Output

OUT

BOOL

TRUE: Input IN is less than input LOW

FALSE: Input IN is greater than input HIGH