Symbol:
Function: This command activates and deactivates the display of interpolation points.
Call: Menu bar:
.Requirement: A CNC path is open in the editor.
If the display of interpolation points is activated, then the CNC path is displayed with interpolation points.
The cycle time, which is set in the dialog box of the CNC settings (Preinterpolation tab), is used for determining the interpolation points In addition, this function determines whether or not a CNC path is displayed with preprocessing in the editor.
See also