Symbol:
Function: The dialog provides parameters for the CNC program object.
Call: Menu bar:
; context menu of the objectRequirement: The CNC object is selected in the device tree.
Application-wide CNC settings are saved in the CNC settings object.
See also
Activate the option to exclude the CNC object from the build. Then IEC data is not generated. However, it is possible to save the G code as an ASCII file. For reading this kind of file at runtime, you can use the function blocks from the SM3_CNC
library.
See also
Implementation |
|
Compile mode |
Behavior on compile
|
File name |
Requirement: Compile mode is set to File. Default: $ObjectName$.cnc. This default value is a placeholder which is replaced by the object name of the CNC object (effective file name) at login. Only the characters [a-zA-Z0-9$_.] are permitted in a file name. The field for the file name must not be blank or start or end with a dot. Moreover, a dot must not be part of the path in the file name. |
Queue size [elements] |
Default: 100. The size setting does not affect the size of the generated |
Default values |
|
Velocity (F) [u/s] |
This value is used when the value of the velocity (in the "F" word) is not set in the CNC program. In path units per second. Value range: [0, 1e9]. Default: 0 |
Acceleration (E+) [u/s²] |
This value is used when the value of the acceleration (in the "E" word with a positive value) is not set. In path units per second squared. Value range: ]0, 1e9]. Default: 100 |
Deceleration (E-) [u/s²] |
This value is used when the value of the deceleration (in the "E" word with a negative value) is not set. In path units per second squared. Value range: ]0, 1e9]. Default: 100 |
Default values for fast forward (G0) |
|
Velocity (FF) [u/s] |
This value is used when the feed value of the velocity (in the "FF" word) is not set in the CNC program. In path units per second. Value range: [0, 1e9]. Default: 0 |
Acceleration (EF+) [u/s²] |
This value is used when the feed value of the acceleration (in the "EF+" word with a positive value) is not set. In path units per second squared. Value range: [0, 1e9]. Default: 0 |
Deceleration (EF-) [u/s²] |
This value is used when the feed value of the deceleration (in the "EF-" word with a negative value) is not set. In path units per second squared. Value range: [0, 1e9]. Default: 0 |
3D-Mode |
Requirement: Implementation Din66025, translation mode CNC_REF, and OUTQueue
|
Offline values of variables |
Variables: If offline values are defined, then the Offline values of variables dialog opens. In this dialog, variables are displayed which can also be edited. |
Start position |
Default: 0 |
See also