The 3-jointed SCARA system has a third axis that allows movement at a constant direction. As for 2-jointed systems, the movement is restricted to the X/Y plane.
See also
SMC_TRAFO_Scara3 (FB)
SMC_TRAFOF_Scara3 (FB)