Function: This command identifies an object and adds it to the "ignore-on-commit” list. Then it is deactivated in the commit dialog by default.
Call: Menu bar:
Requirement: At least one object is available that is not in the change list ignore-on-comment
.
Objects of the "ignore-on-commit” list are overlaid with the symbol in the object tree. By default, they are not selected in the commit dialog, unless a dependency of a selected object requires it. These objects can always be selected manually in the dialog.
See also