Dialog 'Automatic locking failed'

The dialog shows a list of all objects for which an automatic locking was not possible. In the optoins you define how CODESYS SVN will resolve the confilict.

Automatic Locking and Merging
  • Try to steal the lock for the affected objects

  • Activate the "Offline Mode" to temporarily suppress locking

These options are displayed if another user has locked the object.

  • Update the affected objects to the newest revision

  • Update the whole project to the newest revision

  • Activate the "Offline Mode" to temporarily suppress locking

These options are displayed if there exists a more current version of the object on the server.

  • Activate the "Offline Mode" to temporarily suppress locking

These options are displayed if no connection can be established to the server.

SVN Project Settings

Opens the SVN project settings dialog (menu Project ‣ Project Settings ). There you can change the settings for the automatic locking.

SVN Settings

Opens the general SVN project settings dialog (menu Tools ‣ Options ).

See also