Object: EtherCAT Slave
This Tab is for the configuration of the communication settings of the slaves, which support the Ethernet over EtherCAT (EoE).
Requirement:
When using the tvRTSname the installation of the Microsoft Loopback-Adapter as virtual Ethernet adapter is required. A description which explains the installation of this adapter is a available in the internet.
Virtual Ethernet Port |
|
Virtual MAC Id: |
Input field for the Virtual MAC Id |
Switch Port |
|
IP Port |
|
The Ethernet communication parameters must be set according to the parameters of the virtual Ethernet adapter |
|
IP Address |
IP Address of the slave in the network, length: 4 Byte The IP Port must be in the same range as the virtual Ethernet adapter. For example if address of network adapter is 192.168.1.1 and subnet mask is 255.255.255.0 then the IP port must be in the range of 192.168.1.2 to 192.168.1.254 |
Subnet mask |
Subnet mask, length: 4 Byte |
Default Gateway |
Default Gateway, length: 4 Byte |
DNS Server |
IP Address of the DNS server |
DNS Name |
Name of the DNS Server |
See also