Object: EtherNet/IP Adapter
The tab of the device configurator is used for communication between an EtherNet/IP scanner and an EtherNet/IP adapter. The tab shows all device connections from the device description. The user can define a connection tag for each of these device connections.
No additional connections can be added on this tab.
Requirement: This tab is displayed only if the device description contains the parameter ShowTagsPage
and the value of the parameter is set to TRUE
.
Table with the device connections defined in the device description. |
|
Connection Name |
Information originates from the device description Not editable |
Transport Type: |
Information originates from the device description Not editable |
Connection Path |
Information originates from the device description Not editable |
Symbolic Connection Tag |
Connection tag for the connection predefined in the device description. Specified by the user. |
See also