Refer to the general description for information about the following tabs of the device editor.
Only in the case of special features is there an additional help page for the specific device editor.
If the "<device name> Parameters" tab is not shown, then select the Show generic device configuration editors option in the CODESYS options (Device Editor category).
An EtherNet/IP network consists of an EtherNet/IP scanner and one or more EtherNet/IP targets. The scanner thereby represents the master in the network and the targets represent the slaves.
The CODESYS runtime system can act as either a scanner or an adapter.
See also