Function: In this dialog box, you define the alarm classes that are considered for the alarm table or alarm banner.
Call: Property Alarm configuration / Alarm classes of the alarm table or alarm banner visualization element.
Requirement: An alarm table visualization element or alarm banner visualization element is added to the visualization.
Available Alarm Classes |
Shows all alarm classes created in the project. |
Selected Alarm Classes |
The alarm classes in this column are displayed in the alarm table. |
All |
|
|
Moves all available alarm classes to the Selected Alarm Classes column. |
|
Moves the selected alarm classes to the Selected Alarm Classes column. |
|
Removes the selected alarm classes from the Selected Alarm Classes column. |
|
Removes all selected alarm classes from the Selected Alarm Classes column. |
See also