Command 'Interface Editor'
Command 'Keyboard Configuration'
Command 'Visualization Element List'
Command 'Move to Position'
Command 'Reset to Default'
Command 'Activate Keyboard Usage'
Command 'Order'
Command 'Alignment'
Command 'Group'
Command 'Ungroup'
Command 'Frame Selection'
Command 'Background'
Command 'Multiply Visu Element'
Command 'Configure Trace'
Command 'Export Trace Configuration'
Command 'Insert Elements for Controlling Trace'
Command 'Configure Display Settings of the Trend'
Command 'Edit Trend Recording'
Command 'Insert Elements for Controlling the Trend'
Command 'Visualization Element Repository'
Command 'Visualization Style Repository'
Command 'Select Perspective'
Command 'HMI Views'
Command 'Add Visual Element'
Command 'Select None'
Command 'Add Elements for Alarm Acknowledgement'
Command 'Add Elements for Scrolling of Alarms'