Symbol:
Function: This view is used for configuring the element properties of the selected visualization element.
Call: Menu bar:
See also
Column Property |
Element properties of the selected element |
Column Value |
The assigned value is applied in the editor view. |
Double-click in the Value column |
A line editor, drop-down list, or dialog opens for editing the value.
|
Single-click for a selected field |
|
Blank for a selected field |
A style selected in the visualization manager can include single, predefined element properties. As a result, these do not appear in this view because a fixed value is already assigned to them. They do not have to be configured anymore.
Visualizations can be configured with device-specific restrictions that block the availability of element properties.
Device-specific restrictions :
Elements with restricted availability
Fonts with restricted availability
Colors with restricted display
Image formats with restricted display
Maximum number of visualization elements
Maximum number of visualizations below the device