The EcoStruxure Machine Expert project AltivarPLCopenCANopenExample.project provides an application example which shows how to implement an Altivar variable speed drive controlled via fieldbus CANopen. The application example is based on a programming framework supporting general machine control. The monitor and control functions for the Altivar drives are implemented using the PLCopen function blocks from the library GMC Independent PLCopen MC.
System Requirements and Limitations
The application example has been created with the components listed in the table:
Component |
Type and Version |
---|---|
Software |
EcoStruxure Machine Expert V1.1 |
Controller |
TM241CEC24T1) |
Additional devices |
oAltivar 320 oAltivar 340 oAltivar 630 oAltivar 930 All Altivar drives are equipped with the communication module VW3A3608. |
1) This example is based on the Modicon M241 Logic Controller, however, in principle, the concepts for the implementation of the Altivar drives on CANopen are the same for other EcoStruxure Machine Expert controllers. As a precondition, the controller must support the CANopen manager and the GMC Independent PLCopen MC library. |