FUNCTION ResetBusAlarm : ERROR
In case of a Bus Alarm (GetBusAlarm returns TRUE) this function can be called to reset the CAN Hardware.
Scope
Name
Type
Comment
Return
ResetBusAlarm
ERROR
ERROR.NO_ERROR or appropriate error code
Input
hDriver
CAA.HANDLE
handle of CAN interface