CAAReconfigureBase.BeginReconfigure (METH)

METHOD BeginReconfigure

BeginReconfigure has to be called before reconfiguring has been started on the current node. Input itfSender has to be set to the originator node of current reconfiguration (see also input itfSender of IReconfigureProvider.ReconfigureAsync). Note: Each BeginReconfigure must have an CAAReconfigureBase.EndReconfigure call!

InOut:

Scope

Name

Type

Comment

Input

itfSender

INode

itfSender given by IReconfigureProvider.ReconfigureAsync input. If 0 or current node: All enable flags of the current subtree will be updated.