IDevice2.CheckCurrentSupportedCommunicationState (METH)

METHOD CheckCurrentSupportedCommunicationState : BOOL

This method checks if a specific DEVICE_TRANSITION_STATE can be processed in the current state.

Note

Use IDevice2.CheckSupportedCommunicationState to check which DEVICE_TRANSITION_STATE is supported in general.

InOut:

Scope

Name

Type

Comment

Return

CheckCurrentSupportedCommunicationState

BOOL

True if node supports the requested DEVICE_TRANSITION_STATE in the current state.

Input

eRequestedState

DEVICE_TRANSITION_STATE

The communication state to be checked.