| 
NO_ERROR
 | 
0
 | 
no error
 | 
| 
FIRST_ERROR
 | 
1300
 | 
first library-specific error
 | 
| 
TIME_OUT
 | 
1301
 | 
Timeout occured.
 | 
| 
ABORT
 | 
1302
 | 
Operation was aborted.
 | 
| 
REF_INVALID
 | 
1303
 | 
The interface reference was invalid.
 | 
| 
NOT_SUPPORTED
 | 
1304
 | 
The function is not supported.
 | 
| 
ERROR_IO
 | 
1305
 | 
A general I/O configuration error occured.
 | 
| 
PARAM_INVALID
 | 
1306
 | 
Invalid parameter.
 | 
| 
NODE_NOT_EXISTING
 | 
1307
 | 
The specified node does not exist.
 | 
| 
NO_MEMORY
 | 
1308
 | 
Dynamic memory allocation is disabled or system is out of memory.
 | 
| 
ADR_NOT_FOUND
 | 
1309
 | 
The specified I/O address is not valid.
 | 
| 
INST_NOT_FOUND
 | 
1310
 | 
There is no associated IDevice instance for the specified I/O address.
 | 
| 
NO_DATA
 | 
1311
 | 
There is no data available.
 | 
| 
OPERATION_INVALID
 | 
1312
 | 
Operation not possible due to the current state
 | 
| 
FIRST_MF
 | 
1350
 | 
first manufacturer-specific error
 | 
| 
LAST_ERROR
 | 
1399
 | 
last error
 |