Write (FB; Prefix filwr)

FUNCTION_BLOCK Write EXTENDS CBM.ETrigToA

This function block writes data into the file, which was previously opened via ”FILE.Open”. The contents of the memory area indicated by pointer ”pBuffer” should not be modified during the write action! The size of the structure of the memory containing the bytes to be written as well as the number of bytes to be written will not be checked.

If the stability of the pointer on the data structures and their contents cannot be guaranteed in case of an online change, an online change must be avoided with the help of functions from the ”CAA_Application library”.

InOut:

Scope

Name

Type

Comment

Input

hFile

CAA.HANDLE

File handle

pBuffer

CAA.PVOID

The address from where the data can be obtained, can be determined with the help of operator ADR.

szSize

CAA.SIZE

Number of bytes to be written (can be determined via operator SIZEOF)

Output

eError

ERROR

Local library error ID (0: no error; 5101: time out)