FUNCTION_BLOCK Variance
This function will update the experimental variance of the mean with respect to the new input parameter
, which will be added to a series of data
(stemming from previous calls).
The variance
of the data
is calculated according to:
, where
is the arithmetic mean of the data.
| InOut: |
|