ERROR (ENUM)

TYPE ERROR :

This data structure describes errors eventually occurring while working with functions of CAA_SerialCom library. Values ranging from 5000 to 5099 have been reserved for these errors within the prefix registration (LibraryRegistry.chm).

Attributes:

qualified_only

InOut:

Name

Initial

Comment

NO_ERROR

0

no error

FIRST_ERROR

5000

first library specific error

TIME_OUT

5001 = timeout error

ABORT

5002 = abort input active

HANDLE_INVALID

5003 = handle invalid

ERROR_UNKNOWN

5004 = unknown error

WRONG_PARAMETER

5005 = wrong parameter

WRITE_INCOMPLETE

5006 = write incomplete

FIRST_MF

5050

first manufacture specific error

LAST_ERROR

5099

last library specific error