FUNCTION IecTaskReload : RTS_IEC_HANDLE
Reload a specified IEC task. Reload means here: Delete the task at the actual position and create it newly.
|
InOut:
|
|
Scope
|
Name
|
Type
|
Comment
|
|
Return
|
IecTaskReload
|
RTS_IEC_HANDLE
|
Handle to the new created task
|
|
Input
|
hIecTask
|
RTS_IEC_HANDLE
|
Handle to the task to reload
|
|
udiTimeoutMs
|
UDINT
|
|
Timeout in milliseconds to wait, until the task deleted itself. Timeout can be one of the following predefined values:
|
|
See Timeouts details.
|
|
pResult
|
POINTER TO RTS_IEC_RESULT
|
Pointer to error code
|
|