BlockType
|
UINT
|
BlockType
|
BlockLength
|
UINT
|
Length (in bytes) of field AlarmData
|
Version
|
UINT
|
version high + low
|
AlarmType
|
UINT
|
Alarm type
|
API
|
UDINT
|
Application Process Identifier
|
Slot
|
UINT
|
Slot number
|
Subslot
|
UINT
|
Subslot number
|
ModuleIdentNumber
|
UDINT
|
Module Identification number
|
SubmoduleIdentNumber
|
UDINT
|
Submodule Identification number
|
AlarmSpecifier
|
UINT
|
Alarm Specifier
Bit 0 to 10: SequenceNumber
Bit 11: ChannelDiagnosis
Bit 12: ManufacturerSpecificDiagnosis
Bit 13: SubmoduleDiagnosisState
Bit 14: not used
Bit 15: ARDiagnosisState
|
USI
|
UINT
|
UserStructure Identifier
|
AlarmData
|
ARRAY [0..(Constants.MAX_PN_ALARM_DATA - 1)] OF BYTE
|
Alarm information (0..n) bytes)
|